-G num- This option sets the largest size of an object that can be referenced
implicitly with the
gp register. It is only accepted for targets
that use ecoff format. The default value is 8.
-EB-EL- Any mips configuration of
as can select big-endian or
little-endian output at run time (unlike the other gnu development
tools, which must be configured for one or the other). Use ‘-EB’
to select big-endian output, and ‘-EL’ for little-endian.
-KPIC- Generate SVR4-style PIC. This option tells the assembler to generate
SVR4-style position-independent macro expansions. It also tells the
assembler to mark the output file as PIC.
-mvxworks-pic- Generate VxWorks PIC. This option tells the assembler to generate
VxWorks-style position-independent macro expansions.
-mips1-mips2-mips3-mips4-mips5xo-mips32-mips32r2-mips64-mips64r2- Generate code for a particular MIPS Instruction Set Architecture level.
‘-mips1’ corresponds to the r2000 and r3000 processors,
‘-mips2’ to the r6000 processor, ‘-mips3’ to the
r4000 processor, and ‘-mips4’ to the r8000 and
r10000 processors. ‘-mips5’, ‘-mips32’, ‘-mips32r2’,
‘-mips64’, and ‘-mips64r2’
correspond to generic
MIPS V, MIPS32, MIPS32 Release 2, MIPS64,
and MIPS64 Release 2
ISA processors, respectively. You can also switch
instruction sets during the assembly; see Directives to override the ISA level.
-mgp32-mfp32- Some macros have different expansions for 32-bit and 64-bit registers.
The register sizes are normally inferred from the ISA and ABI, but these
flags force a certain group of registers to be treated as 32 bits wide at
all times. ‘-mgp32’ controls the size of general-purpose registers
and ‘-mfp32’ controls the size of floating-point registers.
The .set gp=32 and .set fp=32 directives allow the size
of registers to be changed for parts of an object. The default value is
restored by .set gp=default and .set fp=default.
On some MIPS variants there is a 32-bit mode flag; when this flag is
set, 64-bit instructions generate a trap. Also, some 32-bit OSes only
save the 32-bit registers on a context switch, so it is essential never
to use the 64-bit registers.
-mgp64-mfp64- Assume that 64-bit registers are available. This is provided in the
interests of symmetry with ‘-mgp32’ and ‘-mfp32’.
The .set gp=64 and .set fp=64 directives allow the size
of registers to be changed for parts of an object. The default value is
restored by .set gp=default and .set fp=default.
-mips16-no-mips16- Generate code for the MIPS 16 processor. This is equivalent to putting
.set mips16 at the start of the assembly file. ‘-no-mips16’
turns off this option.
-mmicromips-mno-micromips- Generate code for the microMIPS processor. This is equivalent to putting
.set micromips at the start of the assembly file. ‘-mno-micromips’
turns off this option. This is equivalent to putting .set nomicromips
at the start of the assembly file.
-msmartmips-mno-smartmips- Enables the SmartMIPS extensions to the MIPS32 instruction set, which
provides a number of new instructions which target smartcard and
cryptographic applications. This is equivalent to putting
.set smartmips at the start of the assembly file.
‘-mno-smartmips’ turns off this option.
-mips3d-no-mips3d- Generate code for the MIPS-3D Application Specific Extension.
This tells the assembler to accept MIPS-3D instructions.
‘-no-mips3d’ turns off this option.
-mdmx-no-mdmx- Generate code for the MDMX Application Specific Extension.
This tells the assembler to accept MDMX instructions.
‘-no-mdmx’ turns off this option.
-mdsp-mno-dsp- Generate code for the DSP Release 1 Application Specific Extension.
This tells the assembler to accept DSP Release 1 instructions.
‘-mno-dsp’ turns off this option.
-mdspr2-mno-dspr2- Generate code for the DSP Release 2 Application Specific Extension.
This option implies -mdsp.
This tells the assembler to accept DSP Release 2 instructions.
‘-mno-dspr2’ turns off this option.
-mmt-mno-mt- Generate code for the MT Application Specific Extension.
This tells the assembler to accept MT instructions.
‘-mno-mt’ turns off this option.
-mmcu-mno-mcu- Generate code for the MCU Application Specific Extension.
This tells the assembler to accept MCU instructions.
‘-mno-mcu’ turns off this option.
-minsn32-mno-insn32- Only use 32-bit instruction encodings when generating code for the
microMIPS processor. This option inhibits the use of any 16-bit
instructions. This is equivalent to putting
.set insn32 at
the start of the assembly file. ‘-mno-insn32’ turns off this
option. This is equivalent to putting .set noinsn32 at the
start of the assembly file. By default ‘-mno-insn32’ is
selected, allowing all instructions to be used.
-mfix7000-mno-fix7000- Cause nops to be inserted if the read of the destination register
of an mfhi or mflo instruction occurs in the following two instructions.
-mfix-loongson2f-jump-mno-fix-loongson2f-jump- Eliminate instruction fetch from outside 256M region to work around the
Loongson2F ‘jump’ instructions. Without it, under extreme cases,
the kernel may crash. The issue has been solved in latest processor
batches, but this fix has no side effect to them.
-mfix-loongson2f-nop-mno-fix-loongson2f-nop- Replace nops by
or at,at,zero to work around the Loongson2F
‘nop’ errata. Without it, under extreme cases, cpu might
deadlock. The issue has been solved in latest loongson2f batches, but
this fix has no side effect to them.
-mfix-vr4120-mno-fix-vr4120- Insert nops to work around certain VR4120 errata. This option is
intended to be used on GCC-generated code: it is not designed to catch
all problems in hand-written assembler code.
-mfix-vr4130-mno-fix-vr4130- Insert nops to work around the VR4130 ‘mflo’/‘mfhi’ errata.
-mfix-24k-no-mfix-24k- Insert nops to work around the 24K ‘eret’/‘deret’ errata.
-mfix-cn63xxp1-mno-fix-cn63xxp1- Replace
pref hints 0 - 4 and 6 - 24 with hint 28 to work around
certain CN63XXP1 errata.
-m4010-no-m4010- Generate code for the LSI r4010 chip. This tells the assembler to
accept the r4010 specific instructions (‘addciu’, ‘ffc’,
etc.), and to not schedule ‘nop’ instructions around accesses to
the ‘HI’ and ‘LO’ registers. ‘-no-m4010’ turns off this
option.
-m4650-no-m4650- Generate code for the MIPS r4650 chip. This tells the assembler to accept
the ‘mad’ and ‘madu’ instruction, and to not schedule ‘nop’
instructions around accesses to the ‘HI’ and ‘LO’ registers.
‘-no-m4650’ turns off this option.
-m3900-no-m3900-m4100-no-m4100- For each option ‘-mnnnn’, generate code for the MIPS
rnnnn chip. This tells the assembler to accept instructions
specific to that chip, and to schedule for that chip's hazards.
-march=cpu- Generate code for a particular MIPS cpu. It is exactly equivalent to
‘-mcpu’, except that there are more value of cpu
understood. Valid cpu value are:
2000,
3000,
3900,
4000,
4010,
4100,
4111,
vr4120,
vr4130,
vr4181,
4300,
4400,
4600,
4650,
5000,
rm5200,
rm5230,
rm5231,
rm5261,
rm5721,
vr5400,
vr5500,
6000,
rm7000,
8000,
rm9000,
10000,
12000,
14000,
16000,
4kc,
4km,
4kp,
4ksc,
4kec,
4kem,
4kep,
4ksd,
m4k,
m4kp,
m14k,
m14kc,
m14ke,
m14kec,
24kc,
24kf2_1,
24kf,
24kf1_1,
24kec,
24kef2_1,
24kef,
24kef1_1,
34kc,
34kf2_1,
34kf,
34kf1_1,
74kc,
74kf2_1,
74kf,
74kf1_1,
74kf3_2,
1004kc,
1004kf2_1,
1004kf,
1004kf1_1,
5kc,
5kf,
20kc,
25kf,
sb1,
sb1a,
loongson2e,
loongson2f,
loongson3a,
octeon,
xlr
For compatibility reasons, ‘nx’ and ‘bfx’ are
accepted as synonyms for ‘nf1_1’. These values are
deprecated.
-mtune=cpu- Schedule and tune for a particular MIPS cpu. Valid cpu values are
identical to ‘-march=cpu’.
-mabi=abi- Record which ABI the source code uses. The recognized arguments
are: ‘32’, ‘n32’, ‘o64’, ‘64’ and ‘eabi’.
-msym32-mno-sym32- Equivalent to adding
.set sym32 or .set nosym32 to
the beginning of the assembler input. See MIPS symbol sizes.
-nocpp- This option is ignored. It is accepted for command-line compatibility with
other assemblers, which use it to turn off C style preprocessing. With
gnu
as, there is no need for ‘-nocpp’, because the
gnu assembler itself never runs the C preprocessor.
-msoft-float-mhard-float- Disable or enable floating-point instructions. Note that by default
floating-point instructions are always allowed even with CPU targets
that don't have support for these instructions.
-msingle-float-mdouble-float- Disable or enable double-precision floating-point operations. Note
that by default double-precision floating-point operations are always
allowed even with CPU targets that don't have support for these
operations.
--construct-floats--no-construct-floats- The
--no-construct-floats option disables the construction of
double width floating point constants by loading the two halves of the
value into the two single width floating point registers that make up
the double width register. This feature is useful if the processor
support the FR bit in its status register, and this bit is known (by
the programmer) to be set. This bit prevents the aliasing of the double
width register by the single width registers.
By default --construct-floats is selected, allowing construction
of these floating point constants.
--trap--no-break-
as automatically macro expands certain division and
multiplication instructions to check for overflow and division by zero. This
option causes as to generate code to take a trap exception
rather than a break exception when an error is detected. The trap instructions
are only supported at Instruction Set Architecture level 2 and higher.
--break--no-trap- Generate code to take a break exception rather than a trap exception when an
error is detected. This is the default.
-mpdr-mno-pdr- Control generation of
.pdr sections. Off by default on IRIX, on
elsewhere.
-mshared-mno-shared- When generating code using the Unix calling conventions (selected by
‘-KPIC’ or ‘-mcall_shared’), gas will normally generate code
which can go into a shared library. The ‘-mno-shared’ option
tells gas to generate code which uses the calling convention, but can
not go into a shared library. The resulting code is slightly more
efficient. This option only affects the handling of the
‘.cpload’ and ‘.cpsetup’ pseudo-ops.